AXIS#.TUNING.USERBANDWIDTH

Description

AXIS#.TUNING.USERBANDWIDTH is used to override the AXIS#.TUNING.TARGETBANDWIDTH calculated by the QuickTune feature. If this value is non-zero, AXIS#.TUNING.BANDWIDTH will be set to this value on the next QuickTune execution.

Versions

Action Version Notes
Implemented 02-12-02-000 

-

General Information

Type Read / Write
Units Hz
Range 0.0 to 50.0
Default Value 0
Data Type Double
See Also AXIS#.TUNING.QUICKTUNE.START

AXIS#.TUNING.BANDWIDTH

Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.TUNING.USERBANDWIDTH

5021h

08h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5047

1

5047 (0x13b7)

AXIS1.TUNING.USERBANDWIDTH

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.TUNING.USERBANDWIDTH

5047

Float

Read/Write

-